跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Configuring the TPS-1 For a Host CPU

Last Updated:06/01/2017

Question:

How should the TPS-1 be configured with the TPS Configurator in order to use a host CPU?

Answer:

A host CPU shall be connected via an 8/16-bit parallel or serial interface in combination with the TPS-1. One of these settings has to be set by the TPS Configurator tool to communicate with the host CPU. When no host CPU is used (IO operation mode) at least IO serial or IO parallel operation mode will need to be set by the TPS Configurator tool.
Suitable Products
TPS-1