跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What are the special European characters?

Latest Updated:08/01/2005

Question:

For the UPD16432 LCD driver, what do character codes 0x8b, 0x8c, 0x8d, 0x9b, 0x9c, and 0x9d define?

Answer:

These are special European characters.
Suitable Products
CMOS Operational Amplifiers
Bipolar Operational Amplifiers
CMOS comparators
bipolar comparators