跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

UPD98410: Malfunctions when logical ports not connected to open PHY

Latest Updated:08/01/2005

Question:

For the UPD98410, to what extent do malfunctions occur when logical ports not connected to PHY are open?

Answer:

Malfunctions may occur with one polling operation in the worst case. The extent of malfunctions depends on various factors.
Suitable Products
BD/DVD Recorder
Digital Camcorder
Industrial Network