跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What happen to the data stored in SRAM if the power shuts down?

Latest Updated:03/16/2012

Question:

If the power supply of the SRAM is shut down without a backup battery or super capacitor, what will happen to the data stored in SRAM?

Answer:

SRAM data will be destroyed in this case. If the power supply of the SRAM is reapplied after data has been destroyed, the data changes randomly to ""0"" or ""1“.
Suitable Products
CMOS Operational Amplifiers
Bipolar Operational Amplifiers
CMOS comparators
bipolar comparators
Asynchronous SRAM