跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

If SRAM Vcc drops to a voltage below VccDR min., is there data in SRAM?

Latest Updated:03/16/2012

Question:

If SRAM Vcc drops to a voltage below VccDR min. in the datasheet, can the data in the SRAM be guaranteed?

Answer:

When SRAM Vcc drops below VccDR min. in the datasheet, the data in SRAM may be corrupted, so it is not guaranteed.
Suitable Products
Asynchronous SRAM