跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is my mistake in verifying the pass on my tiny device?

Latest Updated:03/18/2009

Question:

I am having difficulty in getting my program/verify routines to verify/pass on my Tiny device what am I doing wrong ?

Answer:

The most common problem is that the RTS instruction is not allowed during certain stages of the programming/erasing algorithm. Make sure you have the latest manual and are following the flowcharts correctly.
Suitable Products
H8/300H Tiny