跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is the operating humidity for the H8S/2128?

Latest Updated:03/23/2009

Question:

What is the operating humidity for the H8S/2128?

Answer:

There is no specified limit for the operating humidity, but the recommended humidity level for operation is 40% to 80%. Avoid operating in an environment where condensation occurs.
Suitable Products