跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Why do I need to select the bit rate again on inquiry or selection state?

Latest Updated:03/21/2012

Question:

Bit rate settings are automated on the "bit rate adjustment state" in boot mode. Why do I need to select the bit rate again on the "inquiry or selection state"?

Answer:

The bit rate adjustment is usually connected at a low baud rate, which takes time for writing. Resetting to a high-speed baud rate will shorten the writing (communication) time.
The command to speed up the baud rate is the "new bit rate selection (H'3F)" command.
Suitable Products
SH7285, SH7286
SH7243
SH7214, SH7216
SH7231
SH7239, SH7237
SH7146, SH7149
SH7131, SH7132, SH7136, SH7137
SH7083, SH7084, SH7085, SH7086