跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Which registers are initialized by a power-on reset of WDT?

Latest Updated:03/24/2009

Question:

Which registers are initialized by a power-on reset of WDT?

Answer:

FRQCR,WTCNT and WTCSR are not initialized. Other registers depend on a
power-on reset and a manual reset. For details, please refer to register
descriptions of the hardware manual.
Suitable Products
SH7729R
SH7727
SH7709S
SH7706
SH7705