跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Which current consumption does hardware & software mode indicated?

Latest Updated:03/25/2009

Question:

As for the current consumption at the standby mode described in the electrical characteristic section of the hardware manual, which current consumption of the hardware standby mode and the software standby mode is indicated?

Answer:

The current consumption at the standby mode, described in the electrical characteristic section of the hardware manual, indicates the current consumption of both hardware standby mode and the software standby mode.
Suitable Products
SH7065
SH7058
SH7055
SH7050, SH7051
SH7052, SH7053, SH7054
SH7047, SH7049, SH7105, SH7107, SH7109