跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is the flash memory emulation in RAM?

Latest Updated:03/25/2009

Question:

What is the flash memory emulation in RAM?

Answer:

The flash memory emulation in RAM is to emulate the flash memory by overlapping part of its blocks with RAM. If the overlapped area of the flash memory is accessed when executing the application program, the counterpart of the on-chip RAM can automatically be accessed. It is useful, when data is frequently re-written in real time such as adjusting parameters. In addition, it can make rewriting to the flash memory less frequently.
Suitable Products
SH7144, SH7145
SH7065
SH7058
SH7055
SH7050, SH7051
SH7052, SH7053, SH7054
SH7047, SH7049, SH7105, SH7107, SH7109
SH7046, SH7148, SH7101, SH7048, SH7104, SH7106, SH7108
SH7040, SH7041, SH7042, SH7043, SH7044, SH7045
SH7018
SH7014, SH7016, SH7017