跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is Interrupt Exception Processing Vectors and Priorities Table?

Latest Updated:03/25/2009

Question:

I do not understand the interrupts whose interrupt sources are I/O listed in the Interrupt Exception Processing Vectors and Priorities Table in the section of the interrupt controller of the hardware manual.

Answer:

The interrupts whose interrupt sources are I/O (0EI/MTUP0E/MTU0EI) are used in the Port Output Enable function (POE). These interrupts are generated according to the settings of P0E# to P03# pins or the output state of large-current pins. Please refer to "Port Output Enable (POE)" in the section of the multifunction timer pulse unit (MTU) of the hardware manual for details.
Suitable Products
SH7144, SH7145
SH7047, SH7049, SH7105, SH7107, SH7109
SH7046, SH7148, SH7101, SH7048, SH7104, SH7106, SH7108
SH7040, SH7041, SH7042, SH7043, SH7044, SH7045