跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Start boot mode: Delete block, write data into on-chip flash

Latest Updated:04/19/2013

Question:

Is it necessary to delete the block using block erase command before writing the data into the on-chip flash with the program command when starting the boot mode?

Answer:

When starting the boot mode, all blocks of the on-chip flash will be erased automatically before transit to the wait state for program/erase/other commands. Therefore, the erasing operation for the block before writing the first data is not required.
Suitable Products
SH7285, SH7286
SH7243
SH7214, SH7216
SH7231
SH7239, SH7237
SH7211
SH7124, SH7125
SH7147
SH7146, SH7149
SH7131, SH7132, SH7136, SH7137
SH7083, SH7084, SH7085, SH7086