跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

SH7040 wait pin input: What if the setup and hold times are not met ?

Latest Updated:03/18/2009

Question:

SH7040 wait pin input. What happens if the setup and hold times are not met ?

Answer:

In general, if the WAIT input changes between the setup and hold time, it cannot be guarranteed that a WAIT cycle will be inserted by the BSC. There is no danger of latchup in this case however.
Suitable Products
SH7144 Series
SH7047 Series
SH7046 Series
SH7040 Series