跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is there provision in up/down sequence at power on/off to AVcc, Vcc pin?

Latest Updated:03/21/2012

Question:

Is there any prescriptions for up/down sequences at power on/off to the voltage applied to the AVcc pin and the Vcc pin?

Answer:

There is no prescriptions of power-on sequence for AVCC and VCC. Although, a long-term service with the power provided either one of VCC or AVCC will deteriorate the LSI. Power on/off AVCC and VCC at the same time is preferable.
Suitable Products
SH7285, SH7286
SH7243
SH7214, SH7216
SH7231
SH7239, SH7237
SH7146, SH7149
SH7144, SH7145
SH7083, SH7084, SH7085, SH7086
SH7065
SH7058
SH7055
SH7050, SH7051
SH7052, SH7053, SH7054
SH7047, SH7049, SH7105, SH7107, SH7109
SH7046, SH7148, SH7101, SH7048, SH7104, SH7106, SH7108
SH7040, SH7041, SH7042, SH7043, SH7044, SH7045
SH7032, SH7034, SH7034B
SH7018
SH7014, SH7016, SH7017
SH7011