Is the initial value of weak keeper circuit "High" or "Low"?
Latest Updated:03/23/2009
Question:
Is the initial value of weak keeper circuit "High" or "Low"?
Answer:
It is undetermine whether the initial value of holding level in weak keeper circuit is "High" or "Low" .
To hold the level intention to weak keeper circuit, it is necessary to process pull-up and pull-down.
Suitable Products
SH7206 |
SH7619 |