跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is it possible to use other area to execute Write/Erase program?

Latest Updated:03/25/2009

Question:

Is it possible to use the area other than the blocks targeted for rewriting built-in flash memory as an area to execute Write/Erase program?

Answer:

During Write/Erase, it is not possible to read any areas of flash memory.
Write/Erase programs should be placed on built-in RAM or external memory.
Suitable Products
SH7144, SH7145
SH7065
SH7058
SH7055
SH7050, SH7051
SH7052, SH7053, SH7054
SH7047, SH7049, SH7105, SH7107, SH7109
SH7046, SH7148, SH7101, SH7048, SH7104, SH7106, SH7108
SH7040, SH7041, SH7042, SH7043, SH7044, SH7045
SH7018
SH7014, SH7016, SH7017