跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is it possible to use an external USB transceiver to SH7727?

Latest Updated:03/25/2009

Question:

Can an external USB transceiver be used though the USB transceiver is built into the USB host controller and the USB function controller of SH7727?

Answer:

SH7727 can use an external USB transceiver.

It is assumed that the USB transceiver which has the proven evaluation by customers is used, so it has the specification that can use an external USB transceiver

Suitable Products
SH7727
SH7720