跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is it possible to switch between little Endian and big Endian?

Latest Updated:03/25/2009

Question:

Is it possible to switch between little Endian and big Endian?

Answer:

Yes, it is possible to switch between little endian and big endian by designating an MD5 pin.
At the time of a power-on reset, big endian is engaged when MD5 is low; little endian is engaged when MD5 is high.
This designation is effective for the whole address space, however, endians can not be set for every CS space. Besides, please note that you can not switch endians during CPU operation. For details to set endians,see "Endian/Access Size and Data Alignment" in the section of "Bus State Controller" of Hardware Manual.
Suitable Products
SH7729R
SH7727
SH7720
SH7709S
SH7706
SH7705