跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is it possible to carry out delete/write in the on-chip flash memory?

Latest Updated:03/21/2012

Question:

Is it possible to carry out more deletes/writes in the on-chip flash memory than specified in the Section "Flash Memory Characteristics", Chapter "Electrical Characteristics" of the User's Manual: Hardware?

Answer:

The number of times for write/delete specified in the User's Manual: Hardware is on the assumption of guaranteeing all the characteristics including data hold period (10 years) after rewriting. Writing data for the number of times exceeding that specified in the User's Manual is enabled. When the long-term data preservation and guarantee is not necessary such as the time of debugging assessment, write processing can be repeated until rewrite is disabled.
Suitable Products
SH7285, SH7286
SH7243
SH7214, SH7216
SH7231
SH7239, SH7237
SH7146, SH7149
SH7083, SH7084, SH7085, SH7086