跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

In IEBus, can I do the SLVRQ first then the master transmission request?

"Last Updated" copy

Question:

Can the power supply be connected to the VCL pin?

Answer:

Do not connect an external power supply to VCL. This could permanently damage the device.
Suitable Products
SH7254R
SH7253/td>
SH7058
SH7058S, SH7059
SH7055
SH7050, SH7051
SH7052, SH7053, SH7054