跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How to set bit 6 and bit 7 in MCLKCR?

Latest Updated:09/28/2009

Question:

When using an external clock as the clock for the on-chip PHY, how should I set bit 6 and bit 7 in MCLKCR?

Answer:

Any setting is okay, because the MCLKCR settings do not affect an external clock for on-chip PHY. That is, either of these settings are fine.
00: PLL1 output clock
01: PLL1 output clock
Suitable Products
SH7619