跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How to output clock from the CKIO2 pin?

Latest Updated:03/23/2009

Question:

The clock is not output from the CKIO2 pin.

Answer:

Please confirm common control register (CMNCR) CK2DRV bit of bus state controller (BSC). When the CK2DRV bit is "0", the CKIO2 pin becomes a low level output.
Suitable Products
SH7710