跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Does the SDRAM possible to be used as display memory for LCD?

Latest Updated:03/24/2009

Question:

Is only the synchronous DRAM (SDRAM) possible to be used as display memory for LCD?

Answer:

When using LCD controller, the display memory supports only the
synchronous DRAM (SDRAM) connected to the area 3.
Suitable Products
SH7727
SH7720
  • 这篇文章对您有帮助吗?