跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Does reset exception processing start after the bus cycle has ended?

Latest Updated:03/25/2009

Question:

When a reset is input during accessing to the external memory (during a bus cycle), does reset exception processing start after the bus cycle has ended?

Answer:

- Power-on reset
The LSI becomes to be a power-on reset state on receipt of the reset regardless of the completion of a bus cycle, and reset exception processing starts.

- Manual reset
The Bus State Controller continues to operate even in the manual reset status.
When the LSI enters manual reset status in the middle of a bus cycle, manual reset exception processing does not start until the bus cycle has ended.

Suitable Products
SH7144, SH7145
SH7065
SH7058
SH7055
SH7050, SH7051
SH7052, SH7053, SH7054
SH7047, SH7049, SH7105, SH7107, SH7109
SH7040, SH7041, SH7042, SH7043, SH7044, SH7045
SH7032, SH7034, SH7034B
SH7032
SH7020, SH7021
SH7018
SH7014, SH7016, SH7017
SH7011