跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Does MCU operate correctly when set up and hold time aren't satisfied?

Latest Updated:03/21/2012

Question:

When the set up time and hold time are not satisfied by the external WAIT signal input, does the MCU operate correctly?

Answer:

The MCU operates properly even when the setup time and hold time are not satisfied. However, in this case, wait cycle may not be inserted or one extra cycle may be inserted.
Suitable Products
SH7285, SH7286
SH7243
SH7214, SH7216
SH7231
SH7239, SH7237
SH7146, SH7149
SH7144, SH7145
SH7083, SH7084, SH7085, SH7086
SH7047, SH7049, SH7105, SH7107, SH7109
SH7046, SH7148, SH7101, SH7048, SH7104, SH7106, SH7108
SH7040, SH7041, SH7042, SH7043, SH7044, SH7045
SH7032, SH7034, SH7034B
SH7018
SH7014, SH7016, SH7017
SH7011