跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Can the SH-4 PCI bus be connected to +5V?

Latest Updated:03/23/2009

Question:

The SH-4 PCI bus interface is +3.3V. Can the SH-4 PCI bus be connected to +5V?

Answer:

+5V PCI devices cannot be connected. SH-4 is not tolerant of +5V. Please add a buffer tolerant of +5V between +5V device and SH-4.
Suitable Products
SH7751R
SH7751