跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What should I do to M0A15 and M0A14 of RZ/G1 as NC?

Latest Updated:05/09/2016

Question:

When connecting two 2 Gbit (*16) DDR to the 32-bit bus, if A15 and A14 on the DDR side are 2 Gbit (*16) they are treated as NC. What should I do to M0A15 and M0A14 of RZ/G1?

Answer:

It is not necessary to connect to M0A15 and M0A14. When unused, they are treated as open.
Suitable Products
RZ/G