跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Verified Memory Flash Modules with the RZ/T1

Last Updated:09/27/2017

Question:

What are the Flash Memory Modules that have been verified with the RZ/T1?

Answer:

We have verified the following Flash Memory Modules on the Renesas Starter Kit+ for RZ/T1 and other evaluation boards:
 Serial Flash Memory: MX25L51245GMI-10G   (64M bytes)
               MX25L25635FMI-10G   (32M bytes)
               MX25L3235EM2I-10G   (4M bytes)
 NOR Flash Memory:     MX29GL512FLT2I-10Q (64M bytes, 16 bits x 32M words)
Suitable Products
RZ/T1