跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

RZ/T1 Important Notes for the Thumb Instruction Set

Last Updated:09/27/2017

Question:

Are there any important notes in regards to using the Thumb instruction set?

Answer:

The Cortex-R4 architecture is supposed to set the CPU operation mode to ARM instruction mode when an interrupt occurs after coming from a reset.
Therefore, it's not possible to make a program using only the Thumb instruction set – even if you want to.  In other words, you must make a program using both the ARM instruction set and the Thumb instruction set.

With that, make certain to follow these two points:

- Implement the exception vectors using ARM instructions.

- Implement the FIQ/IRQ interrupt handler using ARM instructions. 

Depending on your tool environment, they could be implemented with C source code declaring a dedicated specifier for an interrupt function.

As reference, please refer to our sample program "RZ/T1 Group Initial Settings (r01an2554)" on our web site.

Suitable Products
RZ/T1