Will an overrun error occurs when 2 frames run and 4 frames are set in SPFC?
Latest Updated:06/10/2013
Question:
When four frames are set in SPDCR.SPFC and a receive buffer full interrupt occurs, if by mistake only two frames are read instead of four, will an overrun error occur?
Answer:
Yes, an overrun error will occur.
Suitable Products
RX62N, RX621 |
RX62T |
RX62G |
RX630 |
RX63N, RX631 |
RX63T |
RX210 |
RX220 |
RX110 |
RX111 |