跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is the reference voltage of the A/D converter of RX62T Group?

Latest Updated:05/27/2013

Question:

There is no VREF pin on the 80-pin package of the RX62T Group. What is the reference voltage of the A/D converter in this case?

Answer:

In the 80-pin package, VREF is connected to AVCC internally. Therefore, the voltage supplied to the AVCC pin is the reference voltage of the A/D converter.

 

Suitable Products
RX62T