跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is on-chip ROM (program ROM) (write only)?

Latest Updated:06/20/2013

Question:

What is on-chip ROM (program ROM) (write only)?

Answer:

The on-chip ROM (program ROM) (write only) area is for erasing or rewriting user programs.
To read after a user program has been erased or rewritten, please use the on-chip ROM (program ROM) (read only).
For more information, please refer to the "Configuration of Memory Mats for the ROM" section in the "ROM (Flash Memory for Code Storage)" chapter of the hardware manual.
Suitable Products
RX62N, RX621
RX62T
RX610
RX62G
RX63T