跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Optimization for network connectivity and HMI function

Last Updated:11/13/2017

Question:

It is said that network connectivity and HMI function have been optimized. Which field is this optimization for? What can be realized by this optimization?

Answer:

Renesas has optimized the new RX65N/RX651 MCUs for connected industrial environments.
The new MCUs offer network connectivity and HMI support that makes it possible to:

o Monitor the operating state of machinery from both inside and outside the factory
o Exchange data for making changes to production instructions
o Reprogram the MCU’s memory to update equipment settings

Suitable Products
RX65N, RX651