跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Multi-Functional Timer Pulse Unit Terminal Names

Last Updated:08/25/2017

Question:

What do "-A" and "-B" attached to the name of a multi-functional timer pulse unit terminal represent?

Answer:

Both "-A" and "-B" have the same terminal function, though they are different ports. You can select which terminal to use by changing the register setting. 

For example, "MTCLKC-A" and "MTCLKC-B" can be selected by port function register C (PFCMTU) of TCLKS (the MTCLK terminal selection bit). 
Refer to the PFCMTU for each package in the I/O port chapter of "User's Manual: Hardware"

Suitable Products
RX62G
RX62T
RX62N
RX621
  • 这篇文章对您有帮助吗?