跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is there greater reduction the more peripheral modules there are?

Latest Updated:05/28/2013

Question:

When using the module stop function to stop the function of peripheral modules, can a greater reduction in power be expected the more peripheral modules there are?

Answer:

Yes.
However, the total amount of power that is reduced will depend on the types of peripheral modules that are stopped.
Suitable Products
RX62N, RX621
RX62T
RX610
RX630
RX63N, RX631
RX210
RX220
RX110
RX111