跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is there any setting required if the voltage detection not working?

Latest Updated:06/10/2013

Question:

The voltage detection circuit is not working. Is any special setting required?

Answer:

This product has a register write protection function that protects important registers from being rewritten. To perform settings to a protected register, writing must first be enabled by the above function.

Please refer to the application note "Register Write Protection Setting Example" (R01AN1206EJ) for details on the register write protection functi

Suitable Products
RX210