跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is it possible to enable both transmission and reception at same time?

Latest Updated:01/23/2014

Question:

Is it possible to enable both transmission and reception at the same time for the serial communications interface so that one byte of data can be transmitted and received on loop back?

Answer:

It is possible. The transmitting and receiving sections are independent inside the SCI and full duplex communication can be performed, so transmitted data can be looped back and received.
Suitable Products
RX630
RX63N, RX631
RX210