跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is MD pin only valid when the reset is performed by a pin reset?

Latest Updated:05/27/2013

Question:

The state of the MD pin during a reset can be used to select the operating mode. Is this only valid when the reset is performed by a pin reset?

Answer:

The state of the MD pin during the following types of reset can be used to select the operating mode.
- RES# pin reset
- Power-on reset (POR)
- Voltage-monitoring 0 reset (LVD0) *
*Only reset by LVD0 is valid. Operating mode cannot be changed by reset by LVD1 or LVD2.

 

Suitable Products
RX62N, RX621
RX62T
RX610