跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

In clock synchronous mode, is it possible to invert the clock or delay?

Latest Updated:01/23/2014

Question:

In clock synchronous mode of the serial communications interface, is it possible to invert the clock or delay by half a clock?

Answer:

It is possible if simple SPI mode is used. For details, please see Operation in Simple SPI Mode in the User's Manual: Hardware.
Suitable Products
RX630
RX63N, RX631
RX210