跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How to enter software standby mode?

Latest Updated:05/28/2013

Question:

I cannot enter software standby mode.

Answer:

Set the software standby bit (SBYCR.SSBY) to 1 and the deep software standby bit (DPSBYCR.DPSBY) to 0 (shifts to software standby mode after the WAIT instruction is executed) before executing the WAIT instruction.
Suitable Products
RX62N, RX621
RX62T
RX610
RX630
RX63N, RX631
RX210