跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Does the time of the clock need to be set every time the power is turn on?

Latest Updated:05/28/2013

Question:

Does the time of the real-time clock need to be set every time the power is turned on?

Answer:

Yes, the time needs to be set every time the power is turned on.

*In the RX630/RX631/RX63N Groups, the time does not have to be set again when power is turned on from VBATT operation, because the RTC operates continuously.

Suitable Products
RX62N, RX621
RX630
RX63N, RX631
RX210
RX220
RX110
RX111