跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

(RX210) Can on-chip RAM values be retained during deep software standby mode?

Latest Updated:05/28/2013

Question:

Can on-chip RAM values be retained during deep software standby mode?

Answer:

[RX210 Group]
On-chip RAM values cannot be retained. For details, see Low Power Consumption in the microcontroller user's manual: hardware.

Suitable Products
RX210