跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

When multiple activation factors occur during DTC transfer

Last Updated:01/16/2018

Question:

How will the DTC operate if multiple activation sources are generated during a DTC transfer?

Answer:

When multiple activation sources are generated during a DTC transfer, the activation sources that were generated during the current DTC transfer are put on hold. After the current DTC transfer is completed, the DTC starts transfer of the activation sources that have been put on hold, in order of priority.
Suitable Products
RL78/F13
RL78/F14
RL78/F15
RL78/G14
  • 这篇文章对您有帮助吗?