跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is the simplified I2C of the 78K0R/Kx3?

Last Updated:12/26/2017

Question:

What is the simplified I2C of the 78K0R/Kx3?

Answer:

This is a serial interface that has only functions as a master in the single master mode of the I2C. Since the wait function is not supported, slow slaves cannot be connected.
Suitable Products
RL78 Family
78K Family