跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is it necessary to define an interrupt function for unused interrupt?

Last Updated:12/26/2017

Question:

Is it necessary to define an interrupt function for unused interrupt?

Answer:

When you don't use an interrupt, it is not necessary to define the corresponding interrupt function.
Suitable Products
RL78 Family
78K Family