跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is it OK if the interval during which the reset signal is input lasts several seconds?

Last Updated:12/26/2017

Question:

Is it OK if the interval during which the reset signal is input lasts several seconds?

Answer:

Yes, there is no problem to input the reset signal for a long time in most cases.

When a reset signal is generated after power on, most pins become high-impedance state.
And port functions during the reset period will be disabled.
Therefore, the through-current never flows.

On the other hand, some of the ports are not disabled during the reset period.
For example, in the case of RL78 / G13, P130 outputs low during the reset period.
Please refer to the user's manual and check if these ports cause problems on your system.

Suitable Products
RL78 Family