跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Count operation when timer RD is changed to short cycle

Last Updated:01/16/2018

Question:

How will Timer RD operate if a cycle value that is smaller than the currently set value is set to a counter?

Answer:

When a general register is used, since the cycle value set to the counter does not match with the newly set value, the timer continues to count until it overflows. After that, the counter operates at the changed cycle value.
When a buffer register is used, the timer operates at the changed cycle value after it operates at the current cycle value.

The above mentioned applies to the duty factor.

To change (update) the cycle and duty factor, pay attention to the differences between the general-purpose registers and buffer registers, the values to be changed, and the timing of the change.

Suitable Products
RL78/G14
RL78/F13
RL78/F14
RL78/F15