跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

About illegal memory access detection function

Last Updated:01/16/2018

Question:

Is write access to the data flash memory available when the illegal memory access detection function is enabled?

Answer:

Writing to the data flash area using the data flash library is possible. If an intended write access to the data flash area is attempted by the execution of a CPU instruction, by the DMA, or by the DTC, a reset signal is generated by the illegal memory access detection function.
Suitable Products
RL78/F12
RL78/F13
RL78/F14
RL78/F15
RL78/D1A
RL78/G13
RL78/G14
  • 这篇文章对您有帮助吗?