跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

OS processing can be executed in maskable interrupt servicing?

Latest Updated:12/01/2011

Question:

Is it possible that OS processing will be executed during maskable interrupt servicing?

Answer:

Unless a system call is issued, OS processing will not be executed during maskable interrupt servicing.
Suitable Products
  • 这篇文章对您有帮助吗?